******************************************************************************
               
                    Automation Builder Virtual Demo - Read Me  

******************************************************************************

At first, open the Start.html file in Internet Explorer to view the demo.
Set browser to full screen mode (F11)
As soon as the demo page is open, Main Menu pops up on the left hand side.
The purpose of Main Menu is to navigate easily through the content.

--------------------------------------------------------------------------------
Video Remarks:
--------------------------------------------------------------------------------


	In each video, there are comments explaining the content. Move the cursor away from the video to view them.
	The videos are looping. Press the play button whenever needed.



--------------------------------------------------------------------------------
Overall Structure:
--------------------------------------------------------------------------------


"Main Menu" has four tabs namely  1. Home, 2. Integration, 3. Openness and 4.Productivity.
For both openness and integration, suite (tool and suite features) + solution (applications and how to build these using Automation Builder) are described.


* The "Home" tab shows the basic relation among Integration, Openness and Productivity. 

* "Integration" tab is further devided into 'Suite' and 'Solution'
	
	--> 'Suite' has a short description on the 'Integrated engineering suite'.
	
		It contains the following sub categories and clicking the 'Launch Demo Videos' tab takes the user to the list of following videos.
		--> One installer
		--> Integrated Suite
		--> Project Handling		
		--> Project Life-Cycle support
	
	--> 'Solution' has a short description on 'Integrated solution Engineering'.
	      
		It contains the below sub categories and clicking the 'Launch Demo Videos' tab allows the user to navigate through the list of following videos.
		--> PLC Drive
		--> PLC Progamming Drive
		--> PLC-Panel
		--> PLC-Safety PLC
		--> PLC-servo drives

	
* "Openness" tab is also further devided into 'Suite' and 'Solution'
	
	--> 'Suite' has a short description on the 'Open engineering suite'.
	
	      It contains the following sub categories and clicking the 'Launch Demo Videos' tab takes the user to the list of following videos.
		--> 3rd party integration
		--> C/C++ programming
		--> Bulk Data Import/Export
		--> Bulk device Manipulation
	
	--> 'Solution' has a short description on 'Open solution Engineering'.
	
	      It contains the below sub categories and clicking the 'Launch Demo Videos' tab allows the user to navigate through the list of following videos.
		--> Manifold Communication
		--> Open Drive Integration
		--> ECAD interface for 3rd party devices

	
* "Productivity" tab has a short description about Virtual Commisioning preview.
    
	Clicking the 'Launch Demo Videos' tab allows the user to watch the below two simulation videos.
	--> Robot Cell
	--> Chair-o-plane



--------------------------------------------------------------------------------
Motivation of the Demo:
--------------------------------------------------------------------------------

* Basic idea: make the benefits of Automation Builder more tangible and easy to present
	--> Clear messages 
	--> Demonstrate features that support these messages
 
* Target audience
	--> Sales persons presenting it on a fair or customer event
	--> Users of Automation Builder: LSUs, Trainers, System Integrators, End-customers, 
	 For marketing and sales purpose 



******************************************************************************

2015-10-28 - please send your feedback to: DE-AutomationBuilder.Support@abb.com

******************************************************************************